EtherCAT Error Messages
***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs motion bus displayed in the Information and Logs window window:
Working Counter failure limit exceeded due to failed node response to cyclic commands. Stopping EtherCAT network cyclic communication.Link Error detected! Please, check controller connection.
Slave %s is not responding to acyclic frame. Please, check power supply or connection.
These messages can appear because of these causes:
|
Error |
Case Description |
Results |
|---|---|---|
|
The XML At the EtherCAT initialization phase, the master checks that:
|
|
|
|
|
|
|
|
|
Possible reasons for the working counter error:
|
|
Other Messages Linked to EtherCAT
See Communication and Fieldbus for more information.
This message is displayed if an error or inconsistency is discovered during the parsing of the XML file when the application is started:
Unable to open EtherCAT config file <file-name>
<file-name>:<line>:<column>: <parsing error>